cancel
Showing results for 
Search instead for 
Did you mean: 

R-Link problem

oe
Associate II
Posted on November 18, 2009 at 12:03

R-Link problem

4 REPLIES 4
oe
Associate II
Posted on May 17, 2011 at 13:30

I having major problem with my R-Link from Raisonance.

It works fine with the Reva board, that it come with. But I cant get any other eva bord to work with it.

When I start the debugger, it goes in to run mode, and when I click stop, it response ''out of code'' and PC is FFFFFF somthing...

Is some one having the same problem?

Any soulutions??

Thanks

Ola

st3
Associate II
Posted on May 17, 2011 at 13:30

Have you asked Raisonance?

oe
Associate II
Posted on May 17, 2011 at 13:30

Yes, I have tried, but I have not been able to find any email address to there support.

However i have posted it on to there forum, but I have not get eny respons on the problem.

vincentchoplin9
Associate II
Posted on May 17, 2011 at 13:30

Hi,

We answered on the Raisonance forum several hours ago:

http://raisonance-forum.xsalto.com/viewtopic.php?id=3089

In short, RST and TRST must not be connected, and by default the Olimex board has them connected by a jumper. You just need to remove the jumper and it should work. For sure that worked for other customers who had the same problem.

If that doesn't solve your problem, please answer there and explain the problem with more details. But in any case you cannot honestly claim that you ''have not get eny respons''. ;)

In fact we even answered two times because we cross-posted. :)

The email address for Raisonance support is ''support@raisonance.com''.

But it will get to the same people that answered on the forum. (either Matloub or me)

Best Regards,

Vincent

(Raisonance support)

[ This message was edited by: VincentC on 18-11-2009 16:35 ]