2014-08-16 9:52 AM
Hi,
my experience with serial comunication is very poor, after six months of ''pain'' trying to implement some AHRS algorithms, now i want to port that data to matlab for example, but i need every dataset to be in its own separate row when i send it to serial#define GPIO_RS232_TX GPIO_Pin_6
#define GPIO_RS232_RX GPIO_Pin_7 #define baudrate 9600 void serial_init(){ // serial usart module & pins initialization GPIO_InitTypeDef GPIO_InitStruct; USART_InitTypeDef USART_InitStruct; GPIO_InitStruct.GPIO_Pin = GPIO_RS232_TX | GPIO_RS232_RX ; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_OType = GPIO_OType_OD; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOB, &GPIO_InitStruct); //Pins modules asigment GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_USART1); // Serial TX GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_USART1); // Serial Rx USART_InitStruct.USART_BaudRate = baudrate; // the baudrate is set to the value we passed into this init function USART_InitStruct.USART_WordLength = USART_WordLength_8b;// we want the data frame size to be 8 bits (standard) USART_InitStruct.USART_StopBits = USART_StopBits_1; // we want 1 stop bit (standard) USART_InitStruct.USART_Parity = USART_Parity_No; // we don't want a parity bit (standard) USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; // we don't want flow control (standard) USART_InitStruct.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; // we want to enable the transmitter and the receiver USART_Init(USART1, &USART_InitStruct); // again all the properties are passed to the USART_Init function which takes care of all the bit setting // Usart_interrupt_enable() USART_Cmd(USART1, ENABLE); } //// function just to send data void serial_out(USART_TypeDef* USARTx, volatile char *s){ while(*s){ // wait until data register is empty while( !(USARTx->SR & 0x00000040) ); USART_SendData(USARTx, *s); *s++; } } for example i have 3 sets of chars char txt1; char txt2 char txt3 for each of them i use the serial out function like bellow:serial_out(USART1, txt1);
serial_out(USART1, txt2);serial_out(USART1, txt3); The data is recived by the PC trough a serial-usb converter, and the problem is how to align every character ser in separate row for example i want every txtX on its own raw At the moment if i read the data, they are all on the same row... How can i separte them? My current code using inemo and output via chars and then to serial float RoLl=xEulerAngles.m_fRoll* 0f / 3.141592f; float Pici=xEulerAngles.m_fPitch * 0f / 3.141592f; float YaW=xEulerAngles.m_fYaw * 0f / 3.141592f; //converts to string sprintf(txt1,''%f'',RoLl); sprintf(txt2,''%f'',Pici); sprintf(txt3,''%f'',YaW); //sends the strings to rs-232 serial_out(USART1,txt1); serial_out(USART1,txt2); serial_out(USART1,txt3);2014-08-16 2:28 PM
For single values per line just add a newline ''\n'' to your format statement.
//converts to string
sprintf(txt1,''%f\n'',RoLl); sprintf(txt2,''%f\n'',Pici); sprintf(txt3,''%f\n'',YaW); For multiple values per line it gets messier. You'll need to buffer your output. Awk is a good tool for rearranging ASCII text files.