2013-09-12 2:38 PM
Hi,
I have a quadratutre encoder set up, and it seems to work fine in one direction with the CNT of the timer incrementing correctly. However when the shaft spins the other way, CNT remains zero. How can I increment/decrement CNT when the shaft spins anticlockwise? If CNT decrements, would I have to minus CNT from 65535? How Do I know the direction its spinning? Below is my code;//PA0 TIM5_ch1 = enc a
//PA1 TIM5_ch2 = enc b
// Enable GPIO clock
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA,ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM5,ENABLE);
// PA0 & PA1 for encoder
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_Init(GPIOA,&GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_TIM5);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_TIM5);
//Configure Timer
TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM5, &TIM_TimeBaseStructure);
//Setup quadrature encoder and enable timer
TIM_EncoderInterfaceConfig(TIM5,TIM_EncoderMode_TI12,TIM_ICPolarity_Rising,TIM_ICPolarity_Rising);
TIM_Cmd(TIM5, ENABLE);
TIM5->CNT = 0;
Thanks for your help in advance!
#timer-encoder-qei
2013-09-12 3:54 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.