cancel
Showing results for 
Search instead for 
Did you mean: 

PWM

mosine
Associate II
Posted on July 05, 2013 at 12:20

Hi,

I'm very demoralized to study PWM for stm3220G evaluation board. I need a tutorial/example to understand concepts.

For example: why does gpio_moder configure in AF (alternate function)?

I configured GPIOA1   in my sample project, but I don't see anything with my oscilloscope in that pin (CN1  - 36 PA1| MII_RX_CLK| JP6 open). 

Help me!

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Amel NASRI
ST Employee
Posted on July 09, 2013 at 17:49

Hello,

For synchronization purpose, you can refer to example in the STM32F2 Standard Peripheral library.

There are examples for synchronization in cascade or parallel modes.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on July 09, 2013 at 18:37

Sorry, I really don't under stand the purpose of TIM3, and the use of CC1 which you don't configure.

You have TIM3 clocking at 10 KHz (100us), TIM2 at 1 KHz (1ms).

Couldn't you just count 20 updates of TIM2 to arrive at 50 Hz (20 ms)

Have the default state of CCR1 = 0 (OFF/LOW), set CCR1=1000 for 20 updates (HIGH), then set CCR1=300 for the desired duty (30/70) for 50 updates?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mosine
Associate II
Posted on July 10, 2013 at 10:39

Hi,

thanks clive1. This is a first part of project, and so TIM3 is base timer (other functions in future) and I used TIM2 for PWM. Is there an example with CCR1/2? thanks