Skip to main content
oeliks
Associate III
December 23, 2019
Solved

Pwm vs timer irq - slow 100khz max

  • December 23, 2019
  • 5 replies
  • 1316 views

Hi ! Im generating pwm at 200khz with no problems. But when I use ​timer to generate interrupt I get max 100khz of pulse on pin. No matter if I use HAL_GPIO_Toggle/WritePin or just GPIOx->BSRR. No matter how low value of timer prescaller I use.

​

Output pin set to high speed.​ push pull. No pullup, no pulldown.

​

Why? Software or hardware limitations?

​

STM32f103c8 at 72 MHz of timer clock​.

This topic has been closed for replies.
Best answer by Tesla DeLorean

Would probably want to have the TIM trigger the ADC(s) directly. At higher speeds want the DMA to collect the ADC data. You could then toggle at DMA HT/TC interrupts at a slower rate, but could relate edge of that to TIM pin output.

5 replies

S.Ma
Principal
December 23, 2019

Why not describe what you want to achieve?

Are you trying to generate PWM by just timer interrupt? (both rise and fall edge? = 400 kHz interrupt if 50% duty cycle)?

Tesla DeLorean
Guru
December 23, 2019

You're going to run out of bandwidth. The interrupt has to push/pop context, and the flash memory is fairly slow. You're likely to saturate the processor as you interrupt above 100 KHz

For driving/modulating pulses at high speeds, use the TIM features, and DMA

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
oeliks
oeliksAuthor
Associate III
December 24, 2019

Thanks for answers :)

​

I wanted to generate a pulse to debug with scope.

​​

PWM_IT 200khz, ​generates interrupt (both rising and falling edge) that starts ADC and sets some output pin at the same time, when ADC is ready the pin is reset by ADC interrupt.

​

Wanted to have a visual interpretation of adc conversion time.​

​

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
December 24, 2019

Would probably want to have the TIM trigger the ADC(s) directly. At higher speeds want the DMA to collect the ADC data. You could then toggle at DMA HT/TC interrupts at a slower rate, but could relate edge of that to TIM pin output.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
oeliks
oeliksAuthor
Associate III
December 24, 2019

Thanks. I will try to use DMA. But while I wanted to collect an array of 20 samples at high pulse and 20 at low, and then replace first sample in array with another, than second etc. And avarage it. To get "walking" avarage. I think it will be more complicated than I think :)

​

​Or mabey take 20 samples, avarage it, take next 20 samples, avarage, and avarage this two avarages .... ohhh