Skip to main content
DOstu.1
Associate
October 19, 2021
Solved

PWM stm32f446re bare metal not working (Pin is basically inactive using a multimeter)

  • October 19, 2021
  • 3 replies
  • 1376 views
#define CR1_CEN			(1U<<0)	
 
/* *************** Enabling PA6, PA7 as OUTPUT PINs *************** */
	/* Enabling clock access AHB1EN for GPIOC */
	RCC->AHB1ENR |= (1U<<2);	
 
/* *************** Setup TIMER8 for PWM control *************** */
	/* Enable clock access to tim8 */
 
	RCC->APB2ENR |= (1U<<1);
 
	/* Set PC6 as AF3 for TIM3_CH1 */
	GPIOC->MODER |= (1U << 13);
	GPIOC->MODER &=~ (1U << 12);
 
	/* Choose AF3(0b0011) for PC6 (AFR[1], it's used for pins from 8 to 15) */
	GPIOC->AFR[0] |= (0x3 << 24);	
 
 
/* *************** TIM3 settings for PWM *************** */
 
	/* Set prescaler value */
	TIM8->PSC = 16000 - 1; 
 
	/* Set auto-reload value */
	TIM8->ARR = 100 - 1;	
 
	/* Set CCR1 as a preload value, it's used to determine the DUTY CYCLE	*/
	TIM8->CCR1 = 90;
 
	/* Set CCMR1 for output compare PWM mode 1 */
	TIM8->CCMR1 |= (1U << 6) | (1U << 5); 
 
	/* *************** Compare MODE / interrupt status *************** */
 
	/* Enable use of preload register */
	TIM8->CCMR1 |= (1U<<3); // CCMR1_OC1PE_EN
 
	/* Enable CH1 as Output Compare */
	TIM8->CCER |= (1U<<0); // CC1EEN
 
	/* Enable TIM interrupt */
 //TIM8->DIER |= (1U<<0);
 
	/* Enable TIM interrupt in NVIC */
	//NVIC_EnableIRQ(TIM8_IRQn);
 
	/* Enable timer*/
	TIM8->CR1 |= CR1_CEN;
 

Unfortunately I can't see any change in the voltage level at the output or any change in the frequency level acording to multimeter.

I can't turn on an external LED as well no matter what values i set as DC or PSC etc.

What is wrong with my code?

To note that I tried with TIM1 initially at PA8 and now i switched to TIM8 but nothing changed.

I want to say as well that when I was using TIM1 I could have an high enough voltage output by setting everything for the TIM1 to work but AFR[0] = 0b0001 << 28; And it was odd because I got confused by that thinking that maybe the AFR started from PA1 for some reason. I could light the LED with those settings (but not as much as I'd like)

Since this pwm will be used for a H-Bridge, it's important that it works at higher voltages (at least 3V.. as a pwm)

Thank you!!

This topic has been closed for replies.
Best answer by TDK

TIM8 is an advanced timer (as is TIM1) and has an MOE (main output enable) bit to globally enable PWMs. You'll need to set it.

SET_BIT(TIMx->BDTR, TIM_BDTR_MOE);

3 replies

TDK
TDKBest answer
October 19, 2021

TIM8 is an advanced timer (as is TIM1) and has an MOE (main output enable) bit to globally enable PWMs. You'll need to set it.

SET_BIT(TIMx->BDTR, TIM_BDTR_MOE);

"If you feel a post has answered your question, please click ""Accept as Solution""."
DOstu.1
DOstu.1Author
Associate
October 19, 2021

That's what I was thinking as well but I didn't try. As soon as I can I'll let you know