2021-01-20 3:57 AM
Hello,
Here is code:
Prescale=7;Periode=7999;Pulse=3998;
void PWMControl(unsigned int Freq){
TIM_TimeBaseInitTypeDef TimeStructureure;
TIM_OCInitTypeDef TIMOCStructureure;
TimeStructure.TIM_Prescaler=Prescale;
TimeStructure.TIM_CounterMode=TIM_CounterMode_Up;
TimeStructure.TIM_Period=Period;
TimeStructure.TIM_ClockDivision=TIM_CKD_DIV1;
TimeStructure.TIM_RepetitionCounter=0;
TIM_TimeBaseInit(TIM4, &TimeStructure);
TIM_Cmd(TIM4, ENABLE);
TIMOCStructure.TIM_OCMode=TIM_OCMode_PWM2;
TIMOCStructure.TIM_OutputState=TIM_OutputState_Enable;
TIMOCStructure.TIM_OCPolarity=TIM_OCPolarity_Low;
TIMOCStructure.TIM_Pulse=Pulse;
TIM_OC1Init(TIM4, &TIMOCStructure);
//TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_ITConfig(TIM4,TIM_IT_Update,ENABLE);
}
void TIM4_IRQHandler(){
if (TIM_GetITStatus(TIM4, TIM_IT_Update) != RESET)
{
X=X+1;
TIM_Cmd(TIM4, DISABLE);
TIM_ClearITPendingBit(TIM4, TIM_IT_Update);
}
}The above code generates a 1Khz with 50% duty cycle with interrupt. However, by counting the X variable(TIM4_IRQHandler) each second I should have 1000 pulses but I get 100 pulses each second. I am curious to know what my problem is.
Solved! Go to Solution.
2021-01-20 4:00 PM
How do you observe the X variable from the first program?
It's probably not a long program, can you please post it completely, in a compilable form, exactly as you've tested it (where you've found X to increment by 100 each second)?
JW
2021-01-20 4:55 AM
Try to toggle a pin in the IRQHandler and observe together with the PWM pin on oscilloscope/logic analyzer.
JW
2021-01-20 10:38 AM
Thank you very much for your comment.
I changed my program to
void TIM4_IRQHandler(){
if(X!=1){
X=1;
GPIO_SetBits(GPIOE,GPIO_Pin_13);
}else
{
X=0;
GPIO_ResetBits(GPIOE,GPIO_Pin_13);
}
TIM_ClearITPendingBit(TIM4, TIM_IT_Update);
//TIM_Cmd(TIM4, ENABLE);
}and Here is my output:
and Here is my PWM output
They are the same( my PWM takes 1ms to make a Pulse , and my IRQ Toggle the output at 1ms,Am I right?) my variable is long volatile but it takes the wrong value.
2021-01-20 4:00 PM
How do you observe the X variable from the first program?
It's probably not a long program, can you please post it completely, in a compilable form, exactly as you've tested it (where you've found X to increment by 100 each second)?
JW
2021-02-02 2:32 AM
Thank you very much , it was related to showing the X variable.