2009-07-09 02:02 AM
PWM on PA8 STM32
2011-05-17 03:48 AM
Dear All,
I'm trying to get a 4KHz square wave out of PA8 using TIM1 in PWM mode. I've tried the various keil and st examples based on timer 3 but I having trouble gettting this working on TIM1. Is there something extra I've got to configure on timer 1? Could anyone post some source for this? Thanks2011-05-17 03:48 AM
Suggest that you first configure PA8 as GPIO and toggle. Armed with that success I suspect that you have missed the set-up/enable of some clock.
Look carefully @ the newest TIM1 examples - most I've tried have worked. Check that you have newest version of Keil & that it ''plays'' nicely w/ your code library. Good luck.2011-05-17 03:48 AM
jj,
It was the TIM1 clock enable I'd forgotten! Cheers. :-)2011-05-17 03:48 AM
i am trying to use TIM3 Channel 1 as PWM from PC6 as AF; but the brigthness doesnt change. what am i doing wrong?? pls help...
here is the code: RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM3 , ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; //this pin functions as AF; when remapping GPIO_PinRemapConfig(GPIO_FullRemap_TIM3, ENABLE); /*GPIOC Configuration: TIM3 channel 1 */ /* make sure that C port is opened in RCC*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); TIM_Cmd(TIM3, DISABLE); TIM_ARRPreloadConfig(TIM3, ENABLE); /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 999; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_Channel = TIM_Channel_1; TIM_OCInitStructure.TIM_Pulse = 500; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInit(TIM3, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM3, ENABLE); /* TIM3 enable counter */ TIM_Cmd(TIM3, ENABLE); TIM_SetCompare1(TIM3,0x10);