2015-06-16 1:45 AM
Hi, I want to use the state of a GPIO Pin (It is driving a chip select on an SPI device) to determine that the SPI transfer has completed. I do know about the callback on the CMSIS code, but I'd prefer not to use that.
So, can I read the state of the actual H/W Pin when I have that pin set to Output mode ?. Thanks, Andy #stm32-cmsis2015-06-16 2:37 AM
As the fine manual states (this one is from RM0008 for STM32F1xx, but I doubt others will be different - check yours):
When the I/O Port is programmed as Output:
[...]
The data present on the I/O pin is sampled into the Input Data Register every APB2
clock cycle This has nothing to do with CMSIS. JW