Program STM32F103C8T6 with Eclipse on a Windows 10 machine
OK, I am sold on STM32 big time. The devices I am using are on a development board, but it's the STM32F103C8T6 at the core. It is the same device used to program using STLINK V2 from a discovery board.
When I can program this device, I plan to production run my own board using this device.
What I am having lots of issues with is programming the device with other than the Arduino IDE. I want to use Eclipse on a Windows 10 machine, and maybe use my home Debian Linux server but it has no GUI. I do not want to CLI or Command Line Interface this board for now.
I have gone through numerous tutorials and posts about using OpenOCD with Eclipse, but nothing I have followed has worked.
I am using a STM32 discovery board to program my STM32F103C8T6 and it works fine with Arduino IDE. I want to break out of the Ardiuno IDE though and use Eclipse. I am interested in using my Eclipse Neon 3 build to program everything I have embedded that supports SWD.
I don't want my hand held in doing this. Just a link to a working tutorial would be good enough for me. Advice in addition would be cool, but I know all of you are so busy.
Thank you for your time!
Sincerely,
Hop