cancel
Showing results for 
Search instead for 
Did you mean: 

Program STM32 via serial

kavinkumar
Associate III

Is it possible to program the MCU via Serial using the USART pins (PB6,PB7)????

 

4 REPLIES 4

You can implement any update method you chose.

For the System Loader see application note AN2606 for pin options.

https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

https://git.code.sf.net/p/stm32flash/code is a nice program to talk to AN2606 compatible bootloaders

Andrew Neil
Super User

In addition to the built-in System Loader mentioned by @Tesla DeLorean  - which has certain restrictions - you can write your own loader to use any interface you like on any pins you like

For example, see Application note AN4657STM32 in-application programming (IAP) using the USART:

https://www.st.com/resource/en/application_note/an4657-stm32-inapplication-programming-iap-using-the-usart-stmicroelectronics.pdf

https://www.st.com/en/embedded-software/x-cube-iap-usart.html

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
DrWidget
Associate II

This guy has a very detailed video series on implementing a custom bootloader: https://www.youtube.com/watch?v=jzo7z2gNBgg&list=PLArwqFvBIlwHRgPtsQAhgZavlp42qpkiG&index=1

He covers most of the code in the video, but he also has git repo if you are short on details: https://github.com/Embetronicx/STM32-Bootloader/tree/main