Skip to main content
MPole
Associate
April 16, 2019
Question

Problems with speex on STM32L151CBU6A with 32MHz

  • April 16, 2019
  • 0 replies
  • 526 views

Hello. I've got a problem with Speex decoder. Is it possible to run Speex decoder WIDEBAND 16kHz or ULTRA_WIDEBAND 32MHz on STM32L151CBU6A on 32MHz? Narrowband 8kHz is running perfectly, but it's only 8kHz quality, so I want to have a little better. When I create spx files with speexdrop program I try to set all qualities and complexity but all of them are running bad. There are problems with sample rate - running too low or too high and I hear many noises. The quality is very bad, it's not the voice I wanted to hear. So what can I do to proper decode my speex files or is it possible at all?

This topic has been closed for replies.