2015-10-10 12:52 PM
Hi Everyone,
I am working on OV7670 module (no FIFO) with STM32F407 chip. Due to I want to get image in 640x480 pixels so I try to manual scan (don't use DMCI). I set REG_CLKRC = CLK_EXT and control clock (set LOW/HIGH for PA8) to get data. The result seems good except there is a ''white'' space on top. I can call transparent white space because I still see items.2015-10-13 8:33 PM
Can anybody help me?
BTW, if I use test pattern it is good. Therefore I think problem comes from register. But there are many secret registers with OV7670 :(