2023-10-31 9:09 AM
Hello. I've a problem regarding LSE On stm32l562xx mcu. Sometimes it boots, sometimes it doesn't "90 % of time it generates timeout Error" . and it takes too much time to boot up to 4 seconds. I've tried all your sdk initializations, also tried setting lse drive to all 4 modes but nothing changes. Same behaviour and same time. Below is my initialization code and attached how we connect LSE on our board. Regards
2023-11-13 1:25 PM
Thanks. My mates in production are doing that now and i'll let you know what we found
2024-08-09 12:03 AM
Dear Friend,
Please can you share, if you were succesful with this issue? I am facing very similar one. No problem with design with G0, F4 but now with L5 we are not able to start LSE properly.
Many thank you for any hint.
Jan
2026-04-27 11:07 AM
Hello friends,
I am facing the same issue. Out of 10 PCBs, only one successfully started the RTC crystal using the LSE. I have already tried several adjustments, and what I observe is instability during the startup of the 32.768 kHz crystal.
In my case, the crystal pads are placed very close, almost touching the microcontroller pins. I am currently using 15 pF capacitors, but I have also tested with 5 pF, 8 pF, and 10 pF, and nothing works.
Strangely, some original microcontrollers work, while others do not, making this a difficult situation for mass production.
Any help is greatly appreciated. Thank you
2026-04-27 11:36 AM
Please don't hijack other threads. Start your own thread, stating the hardware/software you are using, exactly what are the observed symptoms (what do you mean by instability, exactly?) versus the expected behaviour, perhaps giving a link to this thread.
JW