problem with i2S full duplex mode with DMA for Rx- stm32f4x
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-01-29 4:03 AM
Posted on January 29, 2014 at 13:03
Hello,
I am new to stm32fx and trying to interface stm32f415 with TI3204 codec, i am operating stm32 in master mode with codec in slave... currently i can not see MCLK being generated by controller i am pasting my current code any help would be highly appreciatedGPIO_InitTypeDef GPIO_InitStructure; GPIO_StructInit(&GPIO_InitStructure); I2S_InitTypeDef I2S_InitType; /* enable clock for I2S peripheral */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3, ENABLE); RCC_I2SCLKConfig(RCC_I2S2CLKSource_PLLI2S); RCC_PLLI2SCmd(ENABLE); /* GPIOA & GPIOC Peripheral clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOC, ENABLE);/* I2S pins */
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = I2S3_SCLK_PIN | I2S3_SD_PIN | I2S3_MCLK_PIN | I2S3_SD_EXT_PIN; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = I2S3_WS_PIN; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Enable alternate functionality of PA4 | PC7 | PC10 | PC12 | PC11 */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SPI3); /* configure I2S port */ SPI_I2S_DeInit(SPI3); I2S_InitType.I2S_AudioFreq = I2S_AudioFreq_48k; I2S_InitType.I2S_MCLKOutput = I2S_MCLKOutput_Enable; I2S_InitType.I2S_DataFormat = I2S_DataFormat_16b; I2S_InitType.I2S_Mode = I2S_Mode_MasterTx; I2S_InitType.I2S_Standard = I2S_Standard_Phillips; I2S_InitType.I2S_CPOL = I2S_CPOL_Low; I2S_Init(SPI3, &I2S_InitType); /* operating I2S3ext as reciever */ I2S_InitType.I2S_Mode = I2S_Mode_MasterRx; /* Configure for full duplex mode */ I2S_FullDuplexConfig(I2S3ext,&I2S_InitType); /* enable both I2S3 as transmitter and I2S3ext as reciever */ I2S_Cmd(SPI3, ENABLE); I2S_Cmd(I2S3ext,ENABLE);DMA_InitTypeDef DMA_InitStructure;
DMA_StructInit(&DMA_InitStructure); DMA_DeInit(DMA1_Stream0); DMA_InitStructure.DMA_Channel = DMA_Channel_3; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(SPI3_BASE + 0x0C); DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&I2SRecieveBuffer; DMA_InitStructure.DMA_BufferSize = I2S3_RX_BUFFER_SIZE; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_Init(DMA1_Stream0, &DMA_InitStructure); /* Enable DMA channel */ DMA_Cmd(DMA1_Stream0, ENABLE); /* enable SPI interrupts to DMA */ SPI_I2S_DMACmd(I2S3ext, SPI_I2S_DMAReq_Rx, ENABLE); SPI_I2S_ITConfig(SPI3, SPI_I2S_IT_RXNE, ENABLE); NVIC_InitTypeDef NVIC_InitStructure; NVIC_PriorityGroupConfig(NVIC_PriorityGroup_3); /* Configure the SPI interrupt priority */ NVIC_InitStructure.NVIC_IRQChannel = SPI3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); #stm32 #dma #i2s #full-duplex
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0