Problem with I2C
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-07-15 4:46 AM
Posted on July 15, 2014 at 13:46
Hello my name is Dani, I'm starting with bus I2C and the microcontroler stm32f103rd, I have made the next code, it doesn't work. I would like to control a light sensor.
The program stops in:while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY));
GPIO_InitTypeDef GPIO_InitStructure;
I2C_InitTypeDef I2C_InitStructure;int main( void )
{ SysTick_Setup(); I2C_DeInit(I2C1); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); /* Configure I2C1 pins: SCL and SDA */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Enable I2C1 reset state */ RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, ENABLE); /* Release I2C1 from reset state */ RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, DISABLE); /* I2C configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = 0x01; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = 100000; I2C_SoftwareResetCmd(I2C1,ENABLE); I2C_SoftwareResetCmd(I2C1,DISABLE); /* Apply I2C configuration after enabling it */ I2C_Cmd(I2C1,ENABLE); I2C_Init(I2C1, &I2C_InitStructure); while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY)); I2C_GenerateSTART(I2C1, ENABLE); /* Send I2C1 START condition */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); /* Test on I2C1 EV5 and clear it */ I2C_Send7bitAddress(I2C1, I2C_SLAVE_ADDRESS7 , I2C_Direction_Transmitter); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); /* Test on EV6 and clear it */ I2C_ClearITPendingBit(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED); I2C_SendData(I2C1, 0x01); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_GenerateSTOP(I2C1, ENABLE); while(!I2C_GetFlagStatus(I2C1, I2C_FLAG_RXNE)); lsb = I2C_ReceiveData(I2C1); I2C_GenerateSTOP(I2C1, ENABLE); } This code works with stm32f103RB but not with stm32f103RD. Thanks in advance.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0