cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with CLASSB STL_ClockStartUpTest

Arrhenius
Associate III

Hi,

  • In the snippet below, comment says select PLL as system clock but in code it is configured as HSE clock which one shall be considered?

  /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 

    clocks dividers */

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;

  if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

  • In CLASSB package 2.3.0, the startup self test is getting failed during cross reference measurement. In the implementation the HAL driver is replaced by custom drivers, whose source is attached in the thread.

Controller: STM32H723ZG

Package: X-CUBE-CLASSB 2.3.0

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0