2012-05-16 02:26 PM
Hello
I have a problem with calculating internal temperature with STM32. When processor VCC is 3.3V everything is ok - temperature is almoast accurate with wide temerature range. But whet processor VCC is below 3V temperature falls much below zero ( -40stC, -100stC etc...). Where can be a problem ? with best regards2012-05-16 04:27 PM
Where can be a problem ?
Perhaps you can provide some details of the measurements and the math, and how you account for the voltage, that way people might be able to make informed suggestions rather than guessing what the problem is.2012-05-17 01:57 AM
Sounds like a problem with the ADC reference voltage.
There is a ADC channel reserved to measure Vref, adjacent to the internal temp. sensor (IN16, IN17). Do you use a package with external Vref pins ?