cancel
Showing results for 
Search instead for 
Did you mean: 

Problem on USART

lorenzo meneghello
Associate II
Posted on March 05, 2017 at 19:53

Hi, 

I'm working on STM32F091 MCU fora the first time and I'm trying to test the USART1 on PF0,1. I have just wrote the code and it works well, but now I can't receive the RXNE interrupt.. the tx line works normally.. if I try to set the port as an input I see the correct logic level on pin so the port works, it seems that the shift register of USART NOT WORK. Any idea?

Thanks.

lorenzo.

20 REPLIES 20
Marek Bílý
Associate II
Posted on June 15, 2017 at 21:33

You maybe use registry view, which clear status registry flag.