2015-09-16 3:47 PM
In stm32l1xx_hal_ad.c in version 1.30 of the STM32Cube library, at line 538, there is a comparison of ScanConvMode to ADC_SCAN_ENABLE.....that works as long as the caller set ScanConvMode to ADC_SCAN_ENABLE rather than the legacy ENABLE, which is defined as a different value. Elsewhere in the library (stm32l1xx_hal_adc.h), there is a check for ADC_SCAN_ENABLE or ENABLE, to support backwards compatibility. I suggest adding a similar check here.
Chuck #adc #stm32l1512015-09-18 6:39 AM
Hi smith.chuck,
''Elsewhere in the library (stm32l1xx_hal_adc.h), there is a check for ADC_SCAN_ENABLE or ENABLE, to support backwards compatibility''
Please, could you precise where is this check exactly, because I can not find it! Thank you -Shahrzad-
2015-09-18 6:52 AM
Your Text Editor's search function must be broken :) Just kidding.
stm32l1xx_hal_adc.h, Line 956:/* Note: Scan mode is compared to ENABLE for legacy purpose, this parameter */
/* is equivalent to ADC_SCAN_ENABLE. */
#define ADC_CR1_SCAN_SET(_SCAN_MODE_) \
(( ((_SCAN_MODE_) == ADC_SCAN_ENABLE) || ((_SCAN_MODE_) == ENABLE) \
)? (ADC_SCAN_ENABLE) : (ADC_SCAN_DISABLE) \
)
2015-09-18 10:04 AM
Hi,
Guys, now I see what you are suggesting :-).Thank you-Shahrzad-2015-09-21 3:54 AM
Hi ,
Your proposal has been forwarded to development team. Thank you for your contribution. -Shahrzad-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.