Solved
printf double precision but getting just single precision
Posted on June 13, 2017 at 08:51
Hello,
I am working on a firmware for the STM32F765.
This MCU was chosen because of its double precision floating point capabilities.I manged to configure the FPU/Compiler (ARM GCC 5.4) to genertate correct DP native assembly instructions.When debugging, I can verify correct DP calculations.The only thing I cannot manage is to printf results in double precision.
I have tried the formatters %f and %lf but on every printf only single precision is printed out (correctly rounded results but with too less digits).I am using newlib speed optimized (NOT nano), but also the lib stdc++ does the same.Has somebody ever seen the printf output in double precision for an embedded ARM Cortex-M7 code with GCC & if yes, how do I get it running ?Thank you in advance,
Gahlen