cancel
Showing results for 
Search instead for 
Did you mean: 

Potencial error in datasheet for STM32F769.

Andrey.St.
Associate II
Posted on October 30, 2016 at 20:01

Good day!

In datasheet DocID029041 Rev 3 for STM32F769:

''1.1 Full compatibility throughout the family

The STM32F765xx, STM32F767xx, STM32F768Ax and STM32F769xx devices are fully pin-to-pin, compatible with the STM32F4xxxx devices, allowing the user to try different  peripherals, and reaching higher performances(higher frequency) for a greater degree of freedom during the development cycle.''

''The STM32F76x LQFP144, LQFP176, LQFP208, TFBGA216, UFBGA176 packages are fully pin to pin compatible with STM32F4xx devices.''

Thats all.

But not write about version with DSI interface - pinout NOT compatable!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on October 31, 2016 at 10:57

Hi andrey.st,

Could you please precise were exactly you find incompatibility between F76x and F4x devices (regarding DSI)?

Based on following

http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/c5/37/9c/1d/a6/09/4e/1a/DM00273119/files/DM00273119.pdf/jcr:content/translations/en.DM00273119.pdf

and

http://www.st.com/content/ccc/resource/technical/document/datasheet/3b/29/4f/55/c0/75/48/70/DM00208574.pdf/files/DM00208574.pdf/jcr:content/translations/en.DM00208574.pdf

, pinouts are compatible for DSI (packages LQFP176 and TFBGA216).

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrey.St.
Associate II
Posted on October 31, 2016 at 13:43

Hi,Mayla!

I had a situation when I wanted to replace STM32F429IIT6 on STM32F769IIT6 (faster clock speed, more memory, etc.)

Read part 1.1 of the documentation where it says that:

''The STM32F76x LQFP144, LQFP176, LQFP208, TFBGA216, UFBGA176 packages are fully pin to pin compatible with STM32F4xx devices.''

However, this conclusion is erroneous because of the DSI unit.

It would therefore be correct to specify in clause 1.1 of this nuance that mutually compatible only under the presence or absence of a DSI unit.

Best regards, Andrey.