Skip to main content
Vu.Andy
Associate III
March 23, 2018
Question

Possible STM library bug in CAN interrupt routine

  • March 23, 2018
  • 1 reply
  • 487 views
Posted on March 23, 2018 at 17:23

I am using STM32F072 device and I am using STM library calls for all my CAN routines.  But I notice that occasionally, the main interrupt routine HAL_CAN_IRQHandler(&hcan) would not get called.

At the end of my HAL_CAN_RxCpltCallback(), I call

  if(HAL_CAN_Receive_IT(CanHandle, CAN_FIFO0) != HAL_OK)

  {

    /* Reception Error */

    _Error_Handler(__FILE__, __LINE__);

  }

so I think my codes are correct.

So what I do is at the end of my main while() loop, I would call : HAL_CAN_Receive_IT(&L_hcan, CAN_FIFO0)

and so far it seems to have solve my problem. 

So I think the possible problem was for whatever reason, the CAN receive IT was disabled somewhere in STM library routine which I am not able to figure it out yet.  I have seen similar issue in I2C library where I intentionally overwhelm

the I2C bus, STM library routine would incorrectly disable I2C interrupt.  And what I did there is similarly call I2C_IT at

the end of my main while() loop and that solved that problem.

Could anyone know where in the code that CAN would disable the Receive IT?

Thanks.

    This topic has been closed for replies.

    1 reply

    Vu.Andy
    Vu.AndyAuthor
    Associate III
    March 23, 2018
    Posted on March 23, 2018 at 17:46

    I also would like to add that in my error call back routine, I also call CAN_receive_IT

    void HAL_CAN_ErrorCallback(CAN_HandleTypeDef *hcan)

    {

      if(HAL_CAN_Receive_IT(&L_hcan, CAN_FIFO0) != HAL_OK)

      {

        /* Reception Error */

        _Error_Handler(__FILE__, __LINE__);

      }

    }

    so I am not sure where interrupt could be disabled.  It could be a timing thing which might be tricky to figure out.