cancel
Showing results for 
Search instead for 
Did you mean: 

FMC Connect

kadir ustun1
Senior
Posted on March 22, 2018 at 10:03

Hello, I want to use SDRAM with STM32F429(lqfp100). How can I connect FMC pins to SDRAM.

Please can you help me ?

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Posted on March 22, 2018 at 12:48

Are there enough pins? Use the data sheet and review the STM32F429I-DISCO schematic to understand connectivity expectations.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 22, 2018 at 13:01

I thing,there are not enough pins. But I must do MCU that has 100 pins(stm32f429)

Posted on March 22, 2018 at 13:22

You're not going to get 10 gallons in a 5 gallon bucket, decide what goal posts you're going to have to move.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 22, 2018 at 13:45

Don't I connect SDRAM to stm32f429 which has 100 pins ?

Posted on March 22, 2018 at 15:16

You said there aren't enough pins? The Data Sheet should confirm this.

The SDRAM and LCD interfaces consume a lot of pins, by necessity. If you want to escape extended functionality you're going to have to pick a part which has enough pins to do that. I can't wave a wand and make that happen.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 22, 2018 at 21:20

actually ı will gui with stm32f429 that has 100 pins on the tft lcd. so ı need to connect SDRAM. but ı don't know between this mcu and SDRAM connection

Posted on March 23, 2018 at 07:24

And can ı do GUI without external SDRAM?

kadir ustun1
Senior
Posted on March 23, 2018 at 08:54

Can ı make GUI without use external SDRAM?

Posted on March 23, 2018 at 08:38

You can not use SDRAM with 'F429 with less than 144 pins.

JW