cancel
Showing results for 
Search instead for 
Did you mean: 

Porting STM32F412 FSMC example to STM32F407 for Driving TFT LCD

roythomas
Associate II
Posted on October 25, 2016 at 16:47

I am trying to port the ''STemWin_HelloWorld'' example in   Applications  section of ''STM32F412G-Discovery'' board  of ''stm32cube_fw_f4_v1130 '' package.

The code is originally for STM32F412G which uses FSMC peripheral to interface to LCD. I am trying to adapt to STM32F407ZET6.

I have chnaged to startup file for my chip as well as the CMSIS file for the 407 family. the clock I brought to same speed as the original example. LED blinking part of this example  is runing ok in my new board. But the FSMC part seems not communication with TFT. I just tried by reading some registers of my LCD controller which is having some values by default. but  FSMC access always returns 0 in my debugger. I am stuck here.

Do we need any chnage in the FSMC code of STM32F412   when the destination is STM32F407? . As far as I can understand the original code uses function names with prefix FMC, but may be because the original code may be from a chip with FMC .Also FMC is only an  enhancement of FSMC and many defines of FMC are just like a wrapper over FSMC parameters.

Any clues for my problem?

#!stm32f4discovery #fsmc #fmc
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
slimen
Senior
Posted on October 25, 2016 at 19:14

Hello,

Looked at

http://www.st.com/content/ccc/resource/technical/document/application_note/85/ad/ef/0f/a3/a6/49/9a/CD00201397.pdf/files/CD00201397.pdf/jcr:content/translations/en.CD00201397.pdf

 it may be helpful for you, to understand how you should configure FSMC to work with an TFT LCD. 

Regards

roythomas
Associate II
Posted on October 26, 2016 at 08:10

I am referrring to that Note. Note uses 100Pin chip . My chip is 144 pin. Somewhere it says the FSMC in those chips have slight difference. But cant figure out still.

Posted on February 20, 2017 at 00:38

I am also using an stm32f407, and I am unable to toggle the Ax pin so that I can write Data to my ili9341 TFT LCD. Can anyone help me out?