2020-03-29 10:41 PM
The sample code uses p256v1 (which seems to actually be p256r1). This curve works well.
I Got PKA to sign correctly using p256k1 with some minor curve updates.
I am having trouble setting up p224r1. Has anyone got curves other that p256 to work?
Tnx
Hedley
2020-04-11 5:17 PM
Fixed it. The hash normalization for 224 was wrong. The padding in my case needed to be in the upper words before the unroll into pka ram.
Hash : SHA256_Hash :=
(16#00#, 16#00#, 16#00#, 16#00#, 16#24#, 16#f0#, 16#37#, 16#06#,
16#1b#, 16#2b#, 16#3b#, 16#5e#, 16#ba#, 16#8c#, 16#d4#, 16#97#,
16#36#, 16#ff#, 16#25#, 16#1f#, 16#f0#, 16#11#, 16#63#, 16#5b#,
16#c3#, 16#c8#, 16#49#, 16#63#, 16#b5#, 16#39#, 16#4f#, 16#f2#);
secp224r1 works fine. I am sure the others will also.
2020-04-19 4:08 PM
All these curves are working:
Test ("secp521r1", 521, H);
Test ("secp384r1", 384, H);
Test ("secp256r1", 256, H);
Test ("secp256k1", 256, H);
Test ("secp128r1", 128, H);
Test ("secp112r1", 112, H);
Test ("secp112r2", 112, H);
Test ("nistp521", 521, H);
Test ("nistp384", 384, H);
Test ("nistp256", 256, H);
Test ("nistp224", 224, H);
Test ("nistp192", 192, H);
Test ("brainpool256r1", 256, H);
Test ("brainpool256t1", 256, H);
Test ("brainpool384r1", 384, H);
Test ("brainpool384t1", 384, H);
This is via an Ada generic:
package body Curve is
procedure Test (Name : String; NB : UInt32; H : ECDSA_HashStr)
is
package EC is new STM32.PKA (Curve_Name => Name, Num_Bits => NB);
use EC;
Result : Boolean;
PrivateKey : ECDSA_KeyStr := Make_Random_Group_String (NClamp => True);
PublicKey : ECDSA_PublicKeyStr := Make_Public_Key_String (PrivateKey);
K : ECDSA_RandStr := Make_Random_Group_String;
Sig : ECDSA_SignatureStr;
begin
Enable_Pka;
Result := ECDSA_Sign (PrivateKey, H, K, Sig);
Result := ECDSA_Valid (PublicKey, H, Sig);
if not Result then
raise Program_Error with "curve fail";
end if;
end Test;
end Curve;
Code is on github: