cancel
Showing results for 
Search instead for 
Did you mean: 

Pin Compatibility between STM32 family ?

antonius
Senior
Posted on September 15, 2013 at 15:17

Guys,

Does STM32F103XX series have a pin compatibility with STM32F105xx, 107xx and 207xx ?

Any ideas will be appreciated,

Thanks
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on September 15, 2013 at 16:25

The pin compatibility of various STM32 family parts is generally quite good, but attention needs to be paid to supply pins, and regulator caps. There are a handful of pins you'd want to be able to strap high/low depending on which part/foot-print is being used.

These topics get some coverage in the Data Manuals, and app notes, and can perhaps be visualized in tools like the

http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1533/PF251717

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Posted on September 16, 2013 at 07:59

You might also want to have a glimpse at ''AN3427 Migrating applications from STM32F1 series to STM32F2 series''

JW

antonius
Senior
Posted on September 26, 2013 at 15:47

I have STM32F1xx board, is it possible for me to use STM32F2xx painlessly ?

thanks

Posted on September 27, 2013 at 14:37

I have STM32F1xx board, is it possible for me to use STM32F2xx painlessly ?

That depends on how considered the original design was, particularly the supply/vcap pins, and perhaps the strapping of a few other. I have a design using an F2, a simple BOM change permits F1 or F4 placement.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
antonius
Senior
Posted on October 09, 2013 at 17:05

Is it possible to use STM32F107 into STM32F103 board ? I saw from the datasheet, they have the same pinout...

thanks