cancel
Showing results for 
Search instead for 
Did you mean: 

Peripheral view while debugging

solomonviveros
Associate II
Posted on May 02, 2013 at 20:52

While working through the projects in the STM32F4Discovery Keil examples, the peripherals aren't available for view like they are when creating a standalone project. I can add a watch point for SPI2[as an example] and I can view the registers that way, but even that isn't always consistent[sometimes the watch point says the entry is out of scope] like I've come to expect when viewing the peripherals within Keil...my guess is I'm missing a system file that maps the peripherals to their respective locations...any input would be much appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 02, 2013 at 20:58

Yes, Keil changed how uVision displays peripherals, I liked the older interface, but it can do invasive things with the status/data registers.

You could ping your support contact at Keil, their forum is a customer one like this one at ST.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..