cancel
Showing results for 
Search instead for 
Did you mean: 

PC14 behaving strangely in STM32L431

SanFides
Associate

Hi,

I am using PC14 in STM32L431 as an output and getting output 1 even if I make the pin Low .

I have connected VBAT pin to VDD . And the PC14 Pin is pulled up with 10K Resister to VDD.

When I check the out put without pull up it is showing 0 ,but the moment it is connected to VDD through 10K it showing High.

VDD is 3.3v

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

The RTC can override the GPIO settings. Are you using RTC?

If not, show values of the relevant GPIOC registers to verify it's configured correctly. Specifically, show the values when the output is set to 0 but you still see a 1 on the output.

If you feel a post has answered your question, please click "Accept as Solution".

PC13, PC14 and PC15 are in the low power domain. The IO cells have minimal drive current.

Per TDK, make sure the RTC isn't taking these for OSC32 IN/OUT, that you don't enable/start LSE

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

Read out and check/post content of RCC_BDCR and RTC registers.

JW