cancel
Showing results for 
Search instead for 
Did you mean: 

Overdriving LSI oscillator by external oscillator

st2399
Associate
Posted on August 23, 2013 at 15:06

Hi everyone,

I overdrive the low-speed internal oscillator by external source with a small offset and small swing.

Where can I find parameters for external clock(without bypassing LSI osc)?

Thanks.

Eugene

#lsi #oscillator
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 23, 2013 at 15:39

Not sure I understand, you should be able to supply an external clock for LSE of up to 1 MHz, but would need to set LSE bypass mode so as not to be driving OSC32_OUT.

Both LSI and LSE can be operated together, or separately.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
st2399
Associate
Posted on August 23, 2013 at 16:12

The oscillator is 32768 Hz. External and internal oscillators are working together.

I meant, is it possible to supply from external oscillator without bypass mode driving the OSC32_IN? 

If it is, where can I find signal parameters for OSC32_IN pin?

Thanks