cancel
Showing results for 
Search instead for 
Did you mean: 

[OTG + documentation] global NAK clear

waclawek.jan
Super User
Posted on August 28, 2017 at 16:44

More.

The description of global NAKclearing for both IN and OUT is a mess reoccurring in several places - in the description of four set/clear bits in DCTL, in the narrative in several subchapters of Operational model chapter, in description of GONAKEFF/GINAKEFF in GINTSTS. Sometimes they are said to be cleared by 'writing to CGxNAK' (which should probably read as 'writing 1 to CGxNAK' - all four bits in DCTL are probably 'read 0, write 0 ignored, write 1 causes action'), sometimes by 'clearing CGxNAK', sometimes by 'clearing SGxNAK'. There is a bizarre mess at one point in the Operational model chapter, where the text calls for ' clear the SGONAK bit in OTG_FS_DCTL', and pseudocode below that reads 'OTG_FS_DCTL = 1 in CGONAK'...

Seriously?

JW

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Khouloud GARSI
ST Employee
Posted on September 13, 2017 at 16:06

Hello Jan,

To clear/set the Global IN/OUT NAK, writing '1' in the CGXNAK/SGONAK is needed.

This precision will be added to the description of those bits on the reference manual.

Khouloud.

Posted on October 02, 2017 at 10:27

In RM0090, GONAKEFF (a OTG_FS_GINTSTS bit) is in two instances misspelled as GOUTNAKEFF.

JW

Posted on October 02, 2017 at 17:36

Hi Jan,

This issue was already reported and will be fixed on next versions of the reference manuals.

Many thanks.

Khouloud.