2009-03-13 04:16 AM
On DAC output range of STM32F103xC/D/E
2011-05-17 04:06 AM
2011-05-17 04:06 AM
RM0008 - P182 (not 184) states 0/4096*VRef
STM32F103x - P99 states that DAC with buffer ON is 0.2 to Vref-0.2 I can not experiment this right now, but I suspect the output buffer on the DAC is not completly ''rail to rail'', by a 0.2V offset both sides. Try this: Output DAC 0, then 1/2 (2048/4096), then max (4096). Try this with the output buffer on, then buffer off (FWLib Ref, P446). You will easily see how this turns out. From my observations factored with my memory (no reliable), with buffer off the output spans from 0 to VREF. Please, try it, and report back here! :p -Relaxe PS: I =really= apreciate people stating where to look when they ask for help. It makes helping them a lot easier :p