2018-07-05 7:51 AM
Hi,
I got new Nucleo-F767ZI board. I created project for Atollic using CubeMX with FreeRTOS and LWIP and I was able to send ping without any problem. Then I try send small UDP datagram each 1s to mz PC, but it was unsuccessful - STM started sending ARP to my PC, my PC respond with proper ARP, but STM instead of sending UDP datagram, it ask again for ARP. I don't know what is set wrong...
Can somebody please provide me simple project for Atollic, which will send UDP datagram? With FreeRTOS or not, it isn't so relevant for me right now.
STM IP: 192.168.122.100
PC IP: 192.168.122.40
#stm32f72018-07-06 4:48 AM
Finally I was able to send UDP data to broadcast, but not to my PC. After some debugging I found that STM32 don't know MAC address of PC, but it doesn't sends ARP automaticly, ie.:
1. MX_LWIP_Init(); delay for 5s, send UDP to PC - don't work
2.
MX_LWIP_Init(); delay for 5s (during this delay I send ping from PC to STM), send UDP to PC - works fine
So ping from PC to STM will update ARP table in STM, but in case that this table is empty (no ping from PC), STM won't send ARP automatically before sending UDP. How can I change this? Is there additional option in CubeMX (I have ARP enabled).