cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO F411RE USB

Marius CO
Associate III
Posted on January 11, 2018 at 02:31

Hello.

NUCLEO F411RE, Workbench generated project, Ubuntu 64 16.04, STCUbeMX , I think is  V1.18

I wired a USB cable to USB-DP (PA12)  USB-DM (PA11) GND and 5V.

I have a usb initialised as simple as instructed.

void MX_USB_DEVICE_Init(void)

    {

    USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

    USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);

    USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);

    USBD_Start(&hUsbDeviceFS);

    }

When I plug in the USB I cannot see the device. I could not find a solution.

[ 1020.672169] usb 2-2: new full-speed USB device number 19 using xhci_hcd

[ 1020.784169] usb 2-2: device descriptor read/64, error -71

[ 1021.000167] usb 2-2: device descriptor read/64, error -71

[ 1021.216158] usb 2-2: new full-speed USB device number 20 using xhci_hcd

[ 1021.216312] usb 2-2: Device not responding to setup address.

[ 1021.420263] usb 2-2: Device not responding to setup address.

[ 1021.624148] usb 2-2: device not accepting address 20, error -71

[ 1021.736140] usb 2-2: new full-speed USB device number 21 using xhci_hcd

[ 1021.736282] usb 2-2: Device not responding to setup address.

[ 1021.940249] usb 2-2: Device not responding to setup address.

[ 1022.144092] usb 2-2: device not accepting address 21, error -71

[ 1022.144128] usb usb2-port2: unable to enumerate USB device
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Marius CO
Associate III
Posted on January 12, 2018 at 03:40

Hi, Thank you. I figure it out meanwhile with help from a HW engineer.

The Nucleos F411re I have has the 8Mhz crystal on the Sllink side. 

On Nucleo side,
  • I removed the SB16MCO 0 ohm resistor on the back close to crystal holes.
  • I soldered a 25 Mhz crystal and the 2 caps C33 and C44  ~15pf where crystal was missing,
  • I changed the clock in hal*.h from 8Mhz to 25Mhz

 sudo dmesg -c

[46594.984255] usb 2-2: new full-speed USB device number 20 using xhci_hcd

[46595.114171] usb 2-2: New USB device found, idVendor=0483, idProduct=5740

[46595.114175] usb 2-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3

[46595.114176] usb 2-2: Product: STM32 Virtual ComPort

[46595.114178] usb 2-2: Manufacturer: STMicroelectronics

[46595.114179] usb 2-2: SerialNumber: 00000000001A

[46595.114784] cdc_acm 2-2:1.0: ttyACM1: USB ACM devic

View solution in original post

2 REPLIES 2
Imen.D
ST Employee
Posted on January 11, 2018 at 15:49

Hello

marrius9876

,

Check if your VCP driver is correctly installed on PC, and try to increase heap and stack sizes.

May be this is due to VBUS sensing it must be set do Disable.

Note: Please use the last version of STM32CubeMx (v4.23)

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Marius CO
Associate III
Posted on January 12, 2018 at 03:40

Hi, Thank you. I figure it out meanwhile with help from a HW engineer.

The Nucleos F411re I have has the 8Mhz crystal on the Sllink side. 

On Nucleo side,
  • I removed the SB16MCO 0 ohm resistor on the back close to crystal holes.
  • I soldered a 25 Mhz crystal and the 2 caps C33 and C44  ~15pf where crystal was missing,
  • I changed the clock in hal*.h from 8Mhz to 25Mhz

 sudo dmesg -c

[46594.984255] usb 2-2: new full-speed USB device number 20 using xhci_hcd

[46595.114171] usb 2-2: New USB device found, idVendor=0483, idProduct=5740

[46595.114175] usb 2-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3

[46595.114176] usb 2-2: Product: STM32 Virtual ComPort

[46595.114178] usb 2-2: Manufacturer: STMicroelectronics

[46595.114179] usb 2-2: SerialNumber: 00000000001A

[46595.114784] cdc_acm 2-2:1.0: ttyACM1: USB ACM devic