Nucleo-f070rb bootloader
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-08-24 10:45 AM
Posted on August 24, 2017 at 19:45
My board is connected with usb-ttl board and I can communicate with uart using HAL drivers. I am trying to connect using STMFlashLoader Demo app from ST but I keep getting No response from the target,...
So far I have tried boot0 pin set to 1 and jump to system flash using code but it seems there is no connection, I see no response from the target on the scope either. I cant find anything in the AN2606 and must be missing some critical piece of information. any help would be great.
Thanks
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0