2018-11-03 11:09 AM
I want to run the NUCLEO-F042K6 on external 3V3 supply. I understand that in this case ST-LINK remains down, and I cannot use its crystal for clocking. I want to use a crystal to clock the MCU.
Looking at the schematic[1], I wonder if I can use the same crystal as the ST-LINK is using (X2) and place it on X1 pads, in this configuration:
X1: NX3225GD 8MHz EXS00A-CG04874
C12: 10pf
C13: 10pf
SB4: open
SB6: open
SB8: open
SB5: closed
SB7: closed
[1]https://www.st.com/content/ccc/resource/technical/document/user_manual/e3/0e/88/05/e8/74/43/a0/DM00231744.pdf/files/DM00231744.pdf/jcr:content/translations/en.DM00231744.pdf
2018-11-03 12:53 PM
That would look to be the correct interpretation, and bridges.
Using 32-pin L4, not F0 here.
2018-11-06 8:12 AM
Thank you, Clive. What confuses me is that the 32-pin package has only one set of of OSC_IN/OSC_OUT pins, while other packages have dedicated OSC32_IN/OSC32_OUT pins for 32kHz low-speed crystals. I want to make sure I'm connecting the right oscillator to the right pins :=)
Does the 32-pn package not support a 32kHz crystal, or can you configure the same pins to accept either kHz or MHz crystals?
2018-11-06 8:22 AM
Perhaps something best discussed with an FAE.
I'm using a 32-pin L4, and here PA0 is CK_IN, and tests there indicate it is not bonded to the OSC_IN pin, but is more architectural.
Given the relatively low cost of the NUCLEO this is the sort of thing I'd test in real-life before committing to a design.
2018-11-06 8:53 AM
How do I get hold of an ST FAE? st.com's "contact us page" is broken. I was hoping an FAE would turn up here and answer my question directly.