cancel
Showing results for 
Search instead for 
Did you mean: 

New to ST Micro

vikram2
Associate II
Posted on February 06, 2009 at 05:01

New to ST Micro

5 REPLIES 5
vikram2
Associate II
Posted on May 17, 2011 at 13:02

Hi All,

I am to tally new to ST Microcontrollers.

We would like to start a new project and selected STM32F103T

Please give suggestions and let me know from where I can start.

I have gone through the datasheet but it is not that helpful.

Where I can get a detal datasheet considering SFRs and internal architecture description.?

Suggestions,Support advice are welcome

-Vikram

sofiene
Associate III
Posted on May 17, 2011 at 13:02

Hi vikram;

Welcome to the STM32 world :).

For the begnning, the datasheet depends on the device that you will work on it. STM32F101x (access line) or STM32F103x(performance line). So you have to download the exact datasheet.

Also you have to download the reference manual that contains all the details of the product, after that you can download the firmware library.

refer to this link:

http://www.st.com/mcu/modules.php?name=Downloads

Select: STM32 (Arm Cortex M3)32-bit Microcontrollers. And select what you want to download: Datasheet, Reference Manual, Firmware, Application note etc...

B.R.

M3allem

[ This message was edited by: M3allem on 06-02-2009 09:27 ]

vikram2
Associate II
Posted on May 17, 2011 at 13:02

Thanks, Can you provide me reference manual link for that part.

The datasheet is with me.

lil-vince
Associate II
Posted on May 17, 2011 at 13:02

Hi Vikram,

See the RM0008 Reference Manual, the Flash Programming Manual and the Cortex M3 Technical Reference Manual for complete information

sofiene
Associate III
Posted on May 17, 2011 at 13:02

Refer to this link:

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&fam=110&doc=60

B.R.

M3allem