cancel
Showing results for 
Search instead for 
Did you mean: 

Need Information of STM32 MCU evaluation boards with more than 132 GPIO pins available for system development.

VSali.18
Associate II

My questions are,

1. Am I using the right kit?

2. Please confirm if it has 140 GPIOs available as spare output pins.

3. Please suggest any alternative if better options available.

4. Where can I get development software and hardware debuggers?

Thank you in advance.

--

Regards,

Vijay

Deatils I got from online sites:

ST Microelectronics:

Evaluation Kit for STM32F207IGT6 Microcontroller.

ARM 32-bit Cortex-M3 CPU

1MB Flash, 128+4 Kbytes SRAM

Processor speed: 120MHz

140 GPIOs upto 60MHz

DevKit1207 Evaluation Kit is a complete development platform for STM32F207IGT6

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

Most boards don't have that many pins free. You'd likely want to look for a breakout board for a 208-pin device.

Might also seriously consider adding an IO Expander (or two), or and FPGA/CPLD type arrangement, or buffers/latches off the external bus.

Keil and IAR work well, and there are several amateurish offerings if you're not invested.

The ST-LINK V3 is a pretty good debug pod, the V2 and Segger ones also very usable.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal

Maybe check onbga packages for stm32l4r like bga169.

To have good solution, you need to add 6 gpios to your minimum, swd for debug, and both oscillators. They can be used as gpio with constrains...

Thank you.

Thank you.