2021-10-17 11:42 PM
I have a custom PCB with a STM32H7A3ZI MCU, and a S27KL0642S27KS0642 Hyperbus RAM.
My code, as well as the app note (AN5050) I'm following sets up the RAM for memory mapped access.
I've checked and rechecked the pinout and configuration, but every time I try to access the memory address of the ram, the chip locks up completely. The debugger looses connection, and the chip won't program, the ST-LINK V2 gives the error message DEV_TARGET_NOT_HALTED.
I was eventually able to reprogram the board by power cycling it while simultainiously forcing the boot pin high with a probe.
The trace lengths are between 0.62in and 0.97in, except for CS which I (perhaps naively) allowed to be 1.3in.
Here's my current setup code:
OSPIM_CfgTypeDef sOspiManagerCfg = {0};
OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};
hospi1.Instance = OCTOSPI1;
hospi1.Init.FifoThreshold = 4;
hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;
hospi1.Init.DeviceSize = 23;
hospi1.Init.ChipSelectHighTime = 1;
hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 2; /* My OCTOSPI1 module is clocked at 200 MHz ==> 100 MHz HyperRAM clock. */
hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
hospi1.Init.ChipSelectBoundary = 0;
hospi1.Init.ClkChipSelectHighTime = 0;
hospi1.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_BYPASSED;
hospi1.Init.MaxTran = 0;
hospi1.Init.Refresh = 100;
if (HAL_OSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
sOspiManagerCfg.ClkPort = 2;
sOspiManagerCfg.DQSPort = 1;
sOspiManagerCfg.NCSPort = 2;
sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_1_LOW;
sOspiManagerCfg.Req2AckTime = 1;
if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
sHyperBusCfg.RWRecoveryTime = 4;
sHyperBusCfg.AccessTime = 6;
sHyperBusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;
sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;
if (HAL_OSPI_HyperbusCfg(&hospi1, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/* Memory-mapped mode setup */
{
OSPI_HyperbusCmdTypeDef sCommand = { 0 };
OSPI_MemoryMappedTypeDef sMemMappedCfg = { 0 };
/* Memory-mapped mode configuration --------------------------------------- */
sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
sCommand.DQSMode = HAL_OSPI_DQS_ENABLE;
sCommand.Address = 0;
sCommand.NbData = 1;
if( HAL_OSPI_HyperbusCmd( &hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE ) != HAL_OK )
{
Error_Handler();
}
sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
if( HAL_OSPI_MemoryMapped( &hospi1, &sMemMappedCfg ) != HAL_OK )
{
Error_Handler();
}
}And my code to test it:
uint32_t testbuffer[200];
__IO uint32_t *OCTOSPI1_MEMMAPPED_ADD = (__IO uint32_t *)(OCTOSPI1_BASE);
uint16_t index;
for (index = 0; index < 200; index++){ //verify that the chip and debugger are working correctly
testbuffer[index] = index*12;
}
for (index = 0; index < 200; index++){
testbuffer[index] = OCTOSPI1_MEMMAPPED_ADD[index]; //try to read from the external ram, execution freezes here
}
for (index = 0; index < 200; index++){
OCTOSPI1_MEMMAPPED_ADD[index] = index*11;
}
for (index = 0; index < 200; index++){
testbuffer[index] = OCTOSPI1_MEMMAPPED_ADD[index];
}Does anyone know how to solve this, or even debug it? I get no errors, just the lock up.
The only thing I haven't tried is slowing the bus down to 10MHz and painstakingly soldering leads onto the signals for a logic analyzer.
I have noticed that if I upload this code to the older board that lacks the RAM chip, it does not lock up, it just reads some random value when accessing the memory location.
Thanks!
Edit:
Well I've found one mistake. In the fine print of the datasheet I noticed: "Tie the CK# input pin to either VccQ or VssQ if not connected to the host controller, but do not leave it floating." ..but I have left it floating. I wonder if this is the issue? Unfortunately it is difficult to fix.
2025-02-24 10:25 AM - edited 2025-02-24 10:40 AM
Hi,
Have you managed to solve this? I am facing the same issue...
However, in my case I know the HW is correct, as the mentioned /CK is grounded on my board + this RAM on a different board, but with the same connections worked before.
I have tried to create an area in the memory using MPU to allow all access from 0x90000000 + 16MB (size of my HyperRAM), but I still get the same error.
I also don't suspect that the issue would be caused by the HyperRAM, because the code gives an error at the:
line in the DelayBlock_Calibration() function from AN5050. It says "Cannot access memory at 0x90000008". After this, the code proceeds to the for cycle and breaks only when mem_addr takes the 0x90000008 value.
I would suspect the HyperRAM breaking the code when the STM would try to communicate with it, unsuccessfully.
Has anyone else perhaps an idea how this could be debugged?
Thank,
kacsaaa