2008-10-27 7:20 AM
Multiple port interrupts on the same pin (PA13 and PC13)
2011-05-17 3:49 AM
Note: All external pending interrupts are reset before going to sleep.
2011-05-17 3:49 AM
I am trying to get both PA13 and PC13 to trigger rising edge interrupts to wake the system from a sleep state with two separate inputs. I have configured both channels, but only PC13 is triggering the interrupt.
I have other wake-triggering interrupts on other pins of Port A, and they work fine. The only one that isn't working is the one that shares the interrupt with Port C on pin 13. My EXTI initialization code is as follows: void EXTI_Configuration(void) { EXTI_InitTypeDef EXTI_InitStructure; //IGNITION INPUT /* Connect Ignition Button EXTI Line to Ignition Button GPIO Pin */ GPIO_EXTILineConfig(GPIO_PortSourceGPIOC, GPIO_PinSource13); /* Configure Key Button EXTI Line to generate an interrupt on rising edge to wake up from standby */ EXTI_InitStructure.EXTI_Line = EXTI_Line13; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); if (AUXILIARY_KEYFOB_ENABLED) { /* Connect Keyfob Button EXTI Lines to Keyfob Button GPIO Pins */ GPIO_EXTILineConfig(GPIO_PortSourceGPIOA, GPIO_PinSource11 | GPIO_PinSource12 | GPIO_PinSource13 | GPIO_PinSource15); //USB AUX 3 INPUT /* Configure Keyfob Button EXTI Line to generate an interrupt on rising edge to wake up from standby */ EXTI_InitStructure.EXTI_Line = EXTI_Line11; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); //USB AUX 4 INPUT /* Configure Keyfob Button EXTI Line to generate an interrupt on rising edge to wake up from standby */ EXTI_InitStructure.EXTI_Line = EXTI_Line12; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); //NEG AUX 2 INPUT /* Configure Keyfob Button EXTI Line to generate an interrupt on rising edge to wake up from standby */ EXTI_InitStructure.EXTI_Line = EXTI_Line13; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); //NEG AUX 1 INPUT /* Configure Keyfob Button EXTI Line to generate an interrupt on rising edge to wake up from standby */ EXTI_InitStructure.EXTI_Line = EXTI_Line15; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); } }