cancel
Showing results for 
Search instead for 
Did you mean: 

MSI calibration and MSICAL register

srdjan
Associate II
Posted on May 27, 2016 at 15:16

Hello,

I'm calibrating my MSI clock when I'm switching frequencies, and I noticed that whenever I write a value to MSITRIM register, MSICAL automatically changes value too. The reference maual states that this is a readonly register, which is factory calibrated, and I would expect that it should have constant value, but it changes based on what I write in the MSITRIM. How is this working? I coudn't find any details in the ref manual.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on May 27, 2016 at 17:16

Hi stokic.srdjan,

This is aligned with MSICAL description in the STM32L4 reference manual (RM0351): 

These bits are initialized at startup with the factory-programmed MSI calibration trim value. When MSITRIM is written, MSICAL is updated with the sum of MSITRIM and the factory trim value.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

srdjan
Associate II
Posted on May 27, 2016 at 17:23

This information is missing from RM0038 STM32L1 Reference manual.

Thank you for your quick reply!

Amel NASRI
ST Employee
Posted on May 30, 2016 at 19:20

Hi stokic.srdjan,

Please note that RM0038 will be updated in order to align MSICAL (and HSICAL) description with the one in RM0351.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.