cancel
Showing results for 
Search instead for 
Did you mean: 

MCU resets after couple hours

Adistrict
Associate II

Hi, everyone

I have a weird problem, my stm32f103c8 chip goes to reset mode(nRST pin voltage goes below 1.5 v) after working for couple hours. The MCU is switching the GPIOB1(frequency is 500KHz). Do you have any suggestion about this issue? Is it a power up problem(could this be because of wrong voltage rise sequence in VDD,VDDA and nRST pines)?

Thanks in advance,

Amir

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Sounds like a design issue.

Does VDDA fall below the POR Threshold?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

What happens to VDD before/as NRST goes low?

What does the RCC->CSR register indicate as the reset source?

If you feel a post has answered your question, please click "Accept as Solution".
Adistrict
Associate II

I'm attaching my hardware document. What seems to be wrong in the design?

That's really a job for you and your colleagues.

Would suggest you observed the failure, whilst measuring the temperature and voltage out of the regulator, and look at the potentials on VDDA/VSSA with respect to the ground elsewhere, and against the NRST. Look also at the input current, and that consumed by the MCU and attached logic

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Piranha
Chief II

What are we supposed to do with a 3D model? And you didn't answer any of the questions asked by Tesla and TDK.

Ok Piranha, sorry about this!! I was testing the board whole time.

And I just attached the CAD file so you can check the file too.

Adistrict
Associate II

I changed the clock source to HSI(PLL MUX : 6, Core frequency : 24MHz).

So far so good, but I'm intended to use an external crystal resonator.

Do you think this is a clock malfunction?(I doubt that GND plane affects crystal waveform due to its capacitive effect)

TDK
Super User

I don't see any answers to the questions above. Attaching a schematic is going to be more useful than the 3D model.

If you feel a post has answered your question, please click "Accept as Solution".

Here you are, I attached all the documents that you need to investigate the project.