cancel
Showing results for 
Search instead for 
Did you mean: 

mcu halt when a Contactor is turned on

mustafa abdalrazeq
Associate II

i have a an stm32f417vgt6 mcu and its connected with ft800 through 30 cm SPI cable

and the ft800 is driving a tft lcd .. the problem is when the mcu turn on or turn off the Contactor

the mcu halt .. can you please help me how to detect the problem and how to solve it and what couse the problem

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
S.Ma
Principal

Bah, just twist the cable to make LVDS like cable.

Try to change the SPEED of the SPI GPIO and possibly put a serial resistor (1kOhm?) if really there are glitches around.

Remember that the parasitics are minimum if the electrical lines cross at 90 degrees (no crosstalk).

mustafa abdalrazeq
Associate II

i will try your opinions and i will respond as soon as i finish them

thank you all

Dvorak.Peter
Senior II

The so called halt is actually a crash.

An external arc interfered with the normal CPU operation.

The easy solution is to move all digital boards to the front panel.