2011-01-07 1:35 PM
MB525 Eval Board CAN Issue
2011-05-17 5:20 AM
Okay,
So here is the answer. This CAN setup cannot handle the speed with which data originates at the transmitter, meaning that the transmit mailboxes are full when subsequent iteration loops try to fill them up so packets are discarded. Adding a condition to check whether transmit mailboxes are empty or not and then transmitting solves the problem. Thanks, E