2009-04-15 07:38 AM
Maximum transfer rate using isochronous tranfers [USB]
2011-05-17 04:09 AM
Hi USB experts, I´ve been trying to use the USB peripheral in isochronous mode.
I´m being able to comunicate properly but I can´t get the transfer rate I need. The problem seems to be with the size of the packet memory area. It size is 512 bytes, and since I´m using 64 bytes for each buffer (TX and RX) of the endpoint 0, there is only 384 bytes left for my double buffered isochronous endpoint. I need to tranfer 288 bytes each frame (one frame per millisecond). Can anyone tell me if this really is a limitation or if there some way to make it? Thanks.2011-05-17 04:09 AM
I´m not an expert, but I´ve been working with isochronous tranfers too.
I think this is really a limitation. :-( But maybe you can save a few bytes if you downsize your control packet to 32 ou 16 bytes.[ This message was edited by: brunoalltest on 11-04-2009 18:04 ]2011-05-17 04:09 AM
I´m not sure whether is possible to send multiple packets in one frame. If you look at ''Table 5-4. Full-speed Isochronous Transaction Limits'' over USB specification revision 2.0, for a data payload of 16 bytes theres a Max transfer of 60 packets achieving a total max bandwith of 960000 bytes/sec.
But I don´t have any idea if I got the idea right neither if it is possible using the STM32. Maybe some user or moderator can tell us if this is possible and explain how to do it. I couln´d find any other informations on the rm0008, um0424 or um0427. Thanks2011-05-17 04:09 AM
I couldn´t find any solution yet.
Please, if anybody can help I´ll appreciate. Thanks