lwip UDP disable CRC
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-30 4:33 PM
Posted on May 31, 2015 at 01:33
Hello!
I am looking for an overhead free solution for UDP data streaming.Today I am able to stream UDP data from SPI->DMA->MEM->ETH, using pbuf by Ref: TaskUdpStreamErr = netbuf_ref(buf, dataPointer, TASK_UDP_STREAM_PACKET_SIZE); // dataPointer is filled by the DMA and shared with the with other tasksThe issue is
that I want to add a one byte header to the UDP packet, but I want to avoid copying from one memory to another AND I want to avoid packet fragmentation.so I tried this hack: TaskUdpStreamErr = netbuf_ref(buf, dataPointer, TASK_UDP_STREAM_PACKET_SIZE + 1); buf->p->flags = 0x80 | (i << 5) | ci; -- And in the low_level_output(): if (q->flags & 0x80) { *((uint8_t*)buffer + bufferoffset) = q->flags; bufferoffset += 1; byteslefttocopy -= 1; }Problem is that it will fail on the CRC... 1. Is there a way to disable the CRC? is it a valid solution?2. What other solution do you suggest?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0