cancel
Showing results for 
Search instead for 
Did you mean: 

LwIP server example for STM32F746 discovery?

LMI2
Lead
Posted on November 21, 2016 at 20:45

I noticed that there are several LwIP examples for the 407. I dont have a suitable 407 discovery board, but I have 746 discovery board with ethernet connector. Only LwIP example for that is useless, It is so complicated that I wont be using it. I could use a simple HTML server.

Is there a larger example packet for the 746 too.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slimen
Senior
Posted on November 25, 2016 at 16:33

Hello,

You may find many examples with STM32756G_EVAL and get inspired from them to develop your application at this path: STM32Cube_FW_F7_V1.5.1\Projects\STM32756G_EVAL\Applications\LwIP

Check this

http://www.carminenoviello.com/2016/01/22/getting-started-stm32-nucleo-f746zg/

, it may helps you.

Regards