cancel
Showing results for 
Search instead for 
Did you mean: 

Load Capacitors Crystals

Marcel Blindu
Associate II

How to prove if the selection of the load capacitors CL1 and CL2 for HSE and LSE Crystals is correct?

Maybe with oscilloscope?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Mon2
Senior III

If your code runs then you are good to go. You can review the example caps used in the ref design and also contact the crystal manufacturer for their feedback on the recommended loading cap values. Often the caps are around 8pf - 25pf and not super critical on their value. Purchase a few different values to experiment and keep the values the same for both legs of the crystal. If really concerned then you can just skip and source a crystal oscillator which is guaranteed to always power up and oscillate. Be sure that pin # 1 (OE) is strapped HIGH to enable the oscillator. Review the datasheet from ST on how to mate an oscillator vs. crystal. With the oscillator, no loading caps are required.