2010-12-25 3:18 AM
Lib PLL configuration wrong for Connectivity Line
2011-05-17 5:19 AM
STOne-32?
2011-05-17 5:19 AM
/* PCLK1 = HCLK */
RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV2; I think that should read PCLK1 = HCLK / 2 Isn't the max clock for APB1 36 MHz, the timers taking an HCLK (APB1 * 2) feed so can get to 72 MHz (AHB), but none of the other peripherals are rated up there.