2025-03-02 12:04 PM - edited 2025-03-02 12:04 PM
I am trying to turn on the LD3 LED (connected to PB3) on the NUCLEO-L031K6 board using direct register access without libraries, but it is not working. The LED does not turn on. I have configured the pin control register, enabled the GPIOB clock, and set pin PB3 as output, but the LED still does not light up.
Here is the code I am using:
// NUCLEO-L031K6
#define PERIPH_BASE (0x40000000UL)
#define AHB_OFFSET (0x00020000UL)
#define AHB_BASE (PERIPH_BASE + AHB_OFFSET)
#define IO_OFFSET (0x10000000UL)
#define IOPORT_BASE (PERIPH_BASE + IO_OFFSET)
#define GPIOB_OFFSET (0x0400UL)
#define GPIOB_BASE (IOPORT_BASE + GPIOB_OFFSET)
#define RCC_OFFSET (0x00021000UL)
#define RCC_BASE (AHB_BASE + RCC_OFFSET)
#define RCC_IOPENR_OFFSET (0x2CUL)
#define RCC_IOPENR (*(volatile unsigned int *)(RCC_BASE + RCC_IOPENR_OFFSET))
#define GPIOPBEN (1U<<1)
#define GPIOBMODER_OFFSET (0x00UL)
#define GPIO_MODER (*(volatile unsigned int *)(GPIOB_BASE + GPIOBMODER_OFFSET))
#define GPIO_ODR_OFFSET (0x14UL)
#define GPIO_ODR (*(volatile unsigned int *)(GPIOB_BASE + GPIO_ODR_OFFSET))
#define GPIOB_PIN3 (1U<<3) // LD3 user LED
int main() {
// Enable GPIOB clock
RCC_IOPENR |= GPIOPBEN;
// Set GPIOB pin 3 as output
GPIO_MODER |= (1U<<6);
GPIO_MODER &=~ (1U<<7);
GPIO_ODR |= GPIOB_PIN3; // Turn on LED (set PB3 to HIGH)
while (1) {
}
}Details:
However, the LED is not turning on. Is there something I'm missing in the configuration?
What I've tried:
What else can I check or correct to turn on the LED on this board?
2025-03-03 12:51 PM
Nothing prevents you from studying the startup files created by CubeMX. At least these are guaranteed to work. That's what I do with the folks during trainings/workshops. I don't think finding typos in address constants brings great educational value.